Other Parts Discussed in Thread: TPS40305
art Number: TPS40305
Hi
I am using TPS40305 in my circuit and the output ripple does not match my calculation. My ripple is around 75mV which is a lot higher than 35mv calculated. What could be the reason, the only difference I can find is the output capacitor ESR, which I look everywhere could not find any with ESR of 60
Inputmax 13v min: 12V output: 5V Imax = 100mohm
Thank you