Hi Team
I am looking for ESD protection at 3.3 and 5V, I have a doubt regarding the selection of part is that if the reverse standoff voltage is 5V then in general clamping voltage will be more than 8V. Then at the ESD event 8 volts will be appearing across pin. In that case, does ESD diode will able to save the pin in case of an ESD event.
Please suggest us parts for GPIO (3.3 and 5V ) and it will be really helpful if you can explain to me how it will save my pin.
Let's say I am using TPD1E1B04 for 3.3V GPIO then at the time of ESD 6 V will come. How it will save my pin and why I should use this.