Hi,
the circuit is as below: we are converting 12V to 5V, we cut all the load on 5V power rail so it's 0 load.
When we float EN pin, we got the waveform below:
yellow-12V input, blue-EN pin, green- 5V output.
by zoom in we get the waveform:
by solder R406=200k, R430=40k, we can get normal start up waveform as below:
yellow-12V input, blue- EN pin, green- 5V output.
Why would floating EN pin cause the ripple of Vout, it looks like it stops and then restart, but floating EN pin should be default enable this device.