Other Parts Discussed in Thread: BQ40Z50, BQ4050, BQ40Z50-R2
Hello TI experts,
I have successfully run learning cycle with max error 1% for 18650 cells. My update status is 0e. I have following questions. I look for answers for both the questions. Big thanks in advance.
1) How do I proceed now ? I have learnt from the Forum that I need to make a Golden image .ggcsv file. Can you please proceed for the steps I need to follow for this?
2) Is it possible that I remove the cell with which I ran the learning cycle and plug-in a new or old cell with same chemistry instead and get information about the cell's SOH/SOC/Impedances ? If yes, how do I proceed for this ? Do I have to run complete learning cycles on all the cells again and again or just one cycle or just discharge/charge ? Is this a time-taking process as I see it or can be shortened?
Please help. Please try to not reply with only reference to TRM of BQ40Z50. Any explanation will be helpful.
Regards,
Moonmoon