Hi Team.
Sep_23_2020_TPSM84824_3.6V_5A_Design_Shintomi.pdf
Regards,
Yuichi.Shintomi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team.
Sep_23_2020_TPSM84824_3.6V_5A_Design_Shintomi.pdf
Regards,
Yuichi.Shintomi
Hi Yuichi,
The one comment I have is the AGND pin appears to be connected to the board ground on the main PCB. The AGND pin is connected to PGND through the module so this connection so AGND does not need to be connected to the board ground on the main PCB.
Besides that the values match WEBENCH so it looks good. The one thing to consider if you have space on the board is to add a placeholder Cff cap in parallel with Rfbt in case you need to optimize the transient response. It can be not populated. If you need to try adding it in, a value I would recommend starting with is something in the range of 47 pF to 68 pF. These values will add a zero in the loop between 339kHz and 234kHz.
Anthony
Hi Anthony,
Sep_24_2020_TPSM84824_3.6V_5A_Design_Shintomi.pdf
Regards,
Yuichi