Other Parts Discussed in Thread: DP83826I
Hello - In looking at the DCP021212D data sheet, it states you can sync up to 8 devices together. I would like to avoid using an external sync circuit so can I use 4 stand alone devices? Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello - In looking at the DCP021212D data sheet, it states you can sync up to 8 devices together. I would like to avoid using an external sync circuit so can I use 4 stand alone devices? Thank you
Hello Dan,
I'm not understanding what you would like to do. Are you trying to leave them all floating or tie them together?
Either way should be fine without an external clock.
Regards,
Alejandro
Thanks for writing back. We've resigned ourselves to wedging some strap resistors into the PCB layout, particularly three, to set the MAC Mode and the PHY address as with your help it has become clear that those few strap resistors are unavoidable and must be included in the already packed PCB layout.
It's just an isolated question for the DP83826I. I want to make sure that when a SMI bit has "R/W,STRAP" in the "Type" column, that means I can overwrite the strap value via SMI.
In the specific case, the bit I am looking at is in register BMCR (register address 0), specifically bit 8 Duplex Mode.
The internal pull-down resistor would default this to "Auto Negotiation Disable" "Speed 10M" "Half-Duplex" mode, which is not what I want, so I would have to overwrite via SMI after the strap values latch. Please advise if I can override these strap values via the SMI.
Unfortunately, I am not aware of that device. That is not part of our coverage of parts. Please open up a new thread with that part number so you can get the proper support. They will get back to you accordingly.
Thanks,
Alejandro
Sorry posted wrong E2E thread before. For the DCP and your initial question, just want to make sure that you can connect up to eight DCP-02's together via syncpin without an external clock
Dan,
I want to make sure I am understanding your question correctly. Your first question was in regards to four DCP02's.
You just stated eight..? Can you please clarify your application/question?
Thanks,
Alejandro