Hello,
does anyone have the efficiency chart for this chip down to 1mA output in a boost converter?
Thank you,
Max
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Max
Just let you know the expert is out of office. Please allow us reply next week. Thanks for your kind understanding.
Hi Max,
I only have the 5Vin/8Vo efficiency at fsw=300kHz.
Eff=86.1% with a 10mA load current;
Eff=48.3% with a 1mA load current;
When operation frequency higher, the efficiency will be lower than the above value.
Now our PHX team support this part. If you want other data, they may help you if they have time.
Hi Noi,
Our expert in PHX team will help to answer your question, they are quite familar with the flyback design.