Tool/software: WEBENCH® Design Tools
Web bench produce a design for an LMZ21701-based step-down converter which calls for a Murata GRM216R71E332KA01D 3.3 nF 1.0 mOhm ESR 25V IRMS 0.0 A 0805 (in) X7R capacitor. This part is obsolete and not available at at least some distributors. I'm trying to determine what part to replace it with. I notice that some possible replacements (e.g. Yaego CC0805KRX7R8BB332 and oters in this series) have either lower ESR at the operating frequency (2.537 MHz) or smaller size. Do I just want the lowest ESR possible, or is it important that it has the specified ESR given in the produced design document? Is it any problem to use a smaller replacement? In particular I'm trying to choose between these four Yaego parts: CC0201KRX7R8BB332 CC0402KRX7R8BB332 CC0603KRX7R8BB332 CC0805KRX7R8BB332. These have size 0201, 0402, 0603 and 0804 (in), and decreasing ESR. Will one of these work and which is best? Thanks