Other Parts Discussed in Thread: BQ24610, BQ40Z50
Dear TI,
The charging current is 16.8V (R25 is changed to about 700 k Ohms) and ISET1 is 2A (R12 is changed to about 3.79k).
It is charged to a lithium battery, but the LED (D7) of STAT1 is flashing.
What is the state of BQ24610 at this time?
Led (D7) flashing (test pin STAT1 waveform) is 200ms lit (LOW) at about 1.73s cycle.
All but stat2 and BATDRV LEDs are lit. In addition, JP settings are short-circuited for JP3:VREF, JP1:OPEN, and other JP.
Best regards,
Kashiki