Other Parts Discussed in Thread: LP87702,
Your company’s LP87702 chip, I read the specification, dual buck+boost, which is more suitable for our company’s mcu+can power supply application scenario.
Our company is input 3.8V~5V, fixed output 3.3V and 1.25V, boost is 3.3V input and 5V output, and the two bucks are required to output 3.3V and 1.25V normally. Now there are the following questions that need your help to confirm
1: I read the specification mentioned that the maximum support current is 3.5A. Does this refer to the total current of 2 bucks or the current of a single buck
2: It is seen in the specification that the EN pin and iic are multiplexed. If it is applied to iic, what is your company's corresponding car gauge model?
3: The reference voltage is not found in the specification, so I don’t know how to set the feedback resistance
4: I see that the dynamic characteristics of buck at 4MHz in the specifications are not very strong. Is there any room for optimization? We hope to reduce it to less than 50mV.
5: This chip of your company has a spread spectrum function. Is spread spectrum enabled by default? What is the spread spectrum range?
6: How much does your company's spread spectrum function optimize EMC? Are there relevant test data and reports?