Other Parts Discussed in Thread: TPS61193, LP8867-Q1
We are using the TI TPS61193 LED DRIVER in our design (In Boost Mode), hence we have some below queries & so please clarify it immediately.
1) To calculate Maximum Power dissipation of Device we need to know internal MOSFET AC switching Loss characteristics, this data is not available in datasheet, hence please get this data for us ASAP.
2) We have doubt whether below formula holds good for calculating the boost output Voltage of VOUT = 42V Max & IOUT = 253mA (Max), VIN = 7.2V (Min) to 15.32V (Max))
Let us know like If we use K=0.88 in calculation is that ok. Whether that requires any schematic change.
3) Need to know how below Typical Application Output Voltage is Calculated from above Formula with R1=750K & R2=130K Ohms.