Is there a specification for the minimum period of voltage input to the SENSE terminal of TPS3899?
If there is a minimum value in the specifications for how long the voltage can be detected below the threshold value, please teach.
I think the device is noise tolerant, so I'm assuming it has a spec for a period of no detection.
・ Is there a value that cannot be detected if the pulse width is less than how many ns?
・ There is no period when it is not detected, and if it falls below even a moment, it will be detected.
===
For example, if the detection threshold voltage is 3.00V,
Suppose that spike noise enters about 10ps at around 3.00V and becomes about 2.9V for a moment.
In this case, it was below the threshold for a period of 10ps.
Will it be reset?
Also, how long will it be treated as invalid?