Dear *,
Please can you review the attached schematic and help answer following questions ?
0) please comment the attached schematic.
1) Can we connect the pin1(NC) to VDD or VSS?
2) Gate driver is used in IIM, can we connect DLH to VDD and DHL to VDD?
3) can we connect the Pin 15 and 14 to HS ?
4) can we connect Pin 11 to HB or HO ?
5) What it the right way to choose BST diode regarding to DC bus voltage if 200V, and what is the min required If for BST diode?
6) In your demo designs why did you use Feed Through Capacitors for the boost capacitor? Can we use standard 0603 BST 1u capacitor for up to 2MHz Fsw and BSC500N20NS3GATMA1 mosfet?
7) How to calculate min input capacitance on VDD pin?
Best Regards,
D.