Hi,
I am trying to use the above part. 5V to 1V when I do a load step I get about 150mV P-P oscillations at about 57KHz on the output and this becomes continuous. There is 180uf of ceramic capacitance directly on the output and then via a zero ohm link a further 70uf of ceramic capacitance and 700uf of tantalum capacitance.
What is the best way of curing this?