Hello I am using TPS61175PWP for boosting voltage from 9-13 V to 12 V.
The input voltage is taken from PV panel which can vary from 9 V to 13 V.
The required output voltage is 12 V.
We are using Typical application circuit provided in product datasheet. Circuit is attached.
My question is when the input voltage is greater than 12 V ( suppose 13V) then this circuit works as buck circuit to regulate input 13 V to 12 Output? Or this circuit can not provide constant 12 V with variable input voltage?
Waiting for kind reply. Thanks