is there a minimum load for the output? I added a 6.8k pull down, to no effect.
The VCC is 12.5V. The Vref is steady at 4.99V.
I can see the RT/CT sawtooth - 427kHz. from pk-pk is from 2V to 3.6V (1.6Vpkpk)
FB pin is 0V
Isense is 0V
COMP is railed out, around 8V.
The output should be 'high' - correct?