This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5008: LM5008

Part Number: LM5008

Hi All

What would be the typical current drain of this device at an input voltage of 17 Vdc?

Regards

ik

  • Hello

    I am afraid you will need to provide more information in order to determine the input current.

    You will need to know the output voltage and the output current.  Also, the switching frequency.

    For moderate to high loads, you would use the effciency curves to estimate the input current:

    Iin=(Vout*Iout)/(Vin*n)  where n = efficiency.

    At light loads it is more dificult to estimate; in this case it is best to measure it.

    Please see the attached paper for more information.

    Thanks

    slyy189.pdf

  • Hello

    I will close this post due to inactivity.

    If you have more questions you can post again.

    Thanks