Hi All,
I was looking for a Buck meet these requirements:
- Vin= 4V-28V
- Vout =3.5V
- Iout= 4A , peak Iout=8A
For Vin=28V,Vout=3.5V, the duty is 12.5%
For Vin=4V,Vout=3.5V, the duty is 87.5%
Can TPS51117 meet these requirement?
Is there any other device fit this situation?
Thanks a lot!