This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25887: BQ25887 Charging Current Measurements

Part Number: BQ25887

Hi!

Having trouble wile measureing charging current with built in ADC. Values read from registers REG1A:REG19 is approx. 20% lower then actual charging current. For example: actual current is 1.082 A, ADC-value is 0.857 A. At lower currents the difference reduses: actual 0.271, read from ADC 0.257 A.

All other parameters including Ibus current are correct.

Thanks for your answers.