This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD87350Q5D: 40V MOS to replace CSD87350Q5D

Part Number: CSD87350Q5D
Other Parts Discussed in Thread: CSD88584Q5DC

Dears

We want to upgrade the CSD87350Q5D with 40V rating, do we have some, P2P is better. thanks

Jun Shen

  • Hi Jun,

    Thanks for the inquiry. Unfortunately, we do not have any 40V power block products that are pin-to-pin compatible with the CSD87350Q5D. Our only 40V power block is the CSD88584Q5DC which is optimized for BLDC motor drive applications switching at up to 50kHz maximum recommended frequency. The other alternative is to use discrete FETs. However, this will be a larger, higher cost solution. Please contact me at my TI email if you would like to discuss further. I am going to close this thread.