Other Parts Discussed in Thread: TPS23734, TPS23734EVM-094, PMP22509, TIDA-00617
Hi,
Could you provide Altium Project Source files of TPS2376H Evaluation Module?
Thanks...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you provide Altium Project Source files of TPS2376H Evaluation Module?
Thanks...
Hello Ahmet,
The TPS2376H is a very old IC (released 2006). We highly discourage this for new designs. This design was released before the IEEE802.3.at standard, that allowed for 25W on the PD. So we highly recommend using an IC released after this standard. Our newest IC, the TPS23734 evaluation module is 5V/5A, same as the TPS2376HEVM.
Here are some of our newer designs that are 5V/5A:
TPS23734EVM-094 (recommended and the gerbers are publicly available)
PMP22509
TIDA-00617
PMP6672
Let me know which one you pick.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments
Hello Michael,
Thank you for useful information. It looks like TIDA-00617 and PMP6672 can be useful for me. Can you send me the design source files of them?
Best Regards
Resolved in private messenger.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments