Hey Team,
I'm using ISO5851 Gate drivers in a 3kW inverter application for a university project.
The gate driver is always low on the fault pin which cannot be reset with a Low input to the fault reset pin.
The operating condition on the logic side of the component is 3.3V referenced to 0V of the microcontroller.
On the driver side VCC is +20V while Vee is -5, Ideal for driving SiC components.
With this in mind I assume that UVLO is not the root cause of the fault.
The Desat Pin has been isolated from the circuit with the voltage at 0 with respect to GND2 yet the fault persists.
Any help here would be Greatly appreciated.
I have attached a Schematic of the Gate Driver circuitry below.