Other Parts Discussed in Thread: TPS55288
Hi All,
TPS63811 input is only 2.2V~5.5V.
Is there any device like TPS63811 which output voltage can set by I2C?
requirements are as fellow:
- Vin=3V~9V
- Vout can set by I2C
- Iout=6A~7A
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Allen:
You can have a look at TPS55288