This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24192: temperature sensing for bq24192

Part Number: BQ24192

Hi team,

My customer  need to set the protection temperature to 0~45 degrees in the design of BQ24192.
Customer saw a recommended values on the spec as follows: RT1: 5.52K; RT2: 31.23K
Since this set of resistance values is relatively rare, they found two sets of close resistance values on the system as follows
RT1: 5.49K / 5.6K; RT2: 31.6K / 30.9K
Please help suggest whether they can choose these two resistors value. Thanks.