Part Number: BQ24192
Hi team,
My customer need to set the protection temperature to 0~45 degrees in the design of BQ24192.
Customer saw a recommended values on the spec as follows: RT1: 5.52K; RT2: 31.23K
Since this set of resistance values is relatively rare, they found two sets of close resistance values on the system as follows
RT1: 5.49K / 5.6K; RT2: 31.6K / 30.9K
Please help suggest whether they can choose these two resistors value. Thanks.