This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088: TPS61088 Application Selection

Part Number: TPS61088
Other Parts Discussed in Thread: LM5155, TPS43061

Dear,Sir

We are having a application to drive the LED Diver,we require a min output voltage of 7V and the current Min of 2A.

The system is operated on the Single cell (Voltage Min 3.6 to 4.2V)configuration of the battery with total capacity of 10Ah around.

Please let us know can we use TPS61088 IC and suggest us some another solution if available.

We are having a constraint of BOM so i would like to keep that Min.

Please help us on the above query..!