This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16030: Voltage crashes momentarily at the output.

Part Number: LMR16030

Hi all,

I have received the boards I designed. I fixed the output voltage to 5.27V.  I use Raspberry pi 3 A + as load.

I am sharing pictures from the oscilloscope.

As you can see it drops to 3 V and raspberry is rebooting.

When using with Raspberry, the voltage drops momentarily. I need urgent help on how to fix this. The power board causes problems in this way while making a demo product.

I also share the link of the product I use.

https://www.digikey.com/en/products/detail/texas-instruments/LMR16030SDDAR/8133146

I also share the schematic.

Regards,

Mehmet