Hi team,
Good day.
Our customer has downloaded the TPS386000QRGPRQ1 3D model in the website, however, the dimension is not the same as the package mechanical data. The height of the model is approx. 1.40mm, whereas the specification states, that the max. height is 1.00mm. Also, the overall dimensions in the 3D model are approx. 4.25mmx4.25mm, while the dimensions in the specification are 4.0mm, and max. of 4.15mm. What is the correct dimension of the device? Do we have a 3D model available with the same dimension shown in the package mechanical data?
Package mechanical data - https://www.ti.com/lit/ml/mpqf126f/mpqf126f.pdf
3D model - vendor.ultralibrarian.com/.../embedded
Regards,
Carlo