Other Parts Discussed in Thread: UCC256404
Hi,
I'm currently debugging a powersupply based on the UCC256304 LLC Controller. Some PCB's (~10%) enter a fault condition after a while for an unknown reason and we're trying to figure out why, more interesting is that when the fault condition occurs it won't recover from it but keeps retrying indefinitely. Attached below are some measurements performed on the circuit when it entered the fault mode. We can see quite clearly that the bootstrap capacitor starts charging when RVCC becomes available but the top MOSFET's gate never goes high (apart from when RVCC is not ready yet as shown in the figure) and thus the switching never begins. We confirmed that the gate of the bottom MOSFET does go high (as the increasing CBoost voltage shows) and that the SS pin charges but as the top FET doesn't start switching the output voltage doesn't increase. The SS pin voltage doesn't cross the FB voltage this way as the FB pin is still high (since the optocoupler is not conducting).
We already established that overtemperature, BLK voltage and RVCC voltage are OK, do you have any guidance as to how we should debug this further or what state the device is in that is won't enable the top gate?
Yellow: RVCC
Purple: CBoost
Blue: Gate voltage of top MOSFET
Green: SS Cap voltage
Figure 1: RVCC ramping
Figure 2: SS ramp
Figure 3: Fault condition loop
With kind regards,
Willem