Other Parts Discussed in Thread: UCC28740
Hi Team,
I would like to get your assistance regarding the design of our customer using UC29811.
- The customer would like to confirm if UC29811 can operate with secondary side voltage detection by using an optocoupler.
In the part of their schematic below, they find that it has ~1V voltage swing that looks like ripple at the output. Also, the circuit seems to reset when EMI is present on the AC input voltage. Do you have any thoughts on how to eliminate these issues?
Only that the schematic differs from the reference design in that part of the input filtering is removed to accommodate measuring the voltage between R3 and R8. They are looking for a solution that would not require that inductor and resistor that were removed.
Looking forward to your input.
Regards,
Jonathan