Hello,
We are worried about using this LED driver.
Can you confirm that the following installation (and use) is possible:
- Vcc: 5V
- Riref: 2kohm for Imax 20mA
- TEST: routed on Vcc
- MODE: routed on Vcc
- GSCLK: routed on GND
- SCLK: pin_cpu
- INS: pin_cpu
- SOUT: pin_cpu
- XLAT: pin_cpu
- BLANK: pin_cpu
- Xerr: Not Used
With this setup, I think I can do this:
- We are in “dot correction” configuration.
- We manage leds On/Off by DCn modification.
- We can change the Led brightness via DCn register.
- I couldn’t control status because I must drive the MODE input...
For simplicity, in our case, we can’t connect GSCLK, so we think we may only use the "dot correction”.
Is-it correct?
Thanks