This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: Dividing EN Voltage

Part Number: TLV62130
Other Parts Discussed in Thread: TPS62135, TPS62147, , TPS62130, TPS3703, TPS3890

Hi team,

As my input voltage ramps up with very slow slew rate 1V/s, the ramp rate at the output is concerned.

So, I'm considering to control the output slew by dividing EN pin voltage.

Should it be OK to divide EN pin for this purpose?

Also, is it ok to use resister value for the divider from kOhms - 10kOhms?

In my use case, VIN=5V and VOUT=3.3V. IOUT=1A.

Regards,

Itoh   

  • Kazuki-San,

    Yes you can use resistor divider at EN pin but if you are looking to enable the TLV62130 at a precise input voltage, then the  TPS62147/8 (2A) or TPS62135/6 (4A) is a good alternative if you want to turn on the IC at a precise input voltage. The EN hi and lo thresholds are tight and that will help you have more control on the precise trigger voltage.

    Thanks,

    Amod

  • Hi Amod-san,

    Thank you so much for your suggestion!

    Could you please check the max. and typ. values of high level EN threshold voltage for TPS62130 and TPS62147/8 respectively?

    Regards,

    Itoh

  • Itoh-san,

    For TPS62130, the max EN VH and min EN VL is not present in the datasheet and internal system. This device has the other thresholds specified in the datasheet. For registering logic HI at EN, you need to ensure you are higher than 0.9V and to register logic low ensure you are below 0.3V.

    The TPS62147/8 has precise EN feature that allows more control on trigger point. EN thresholds are specified in datasheet as well.

    Hope this helps!

    Thanks,

    Amod

  • Thanks for your reply.

    Are TPS62130 specifications for EN pin equal to that of TLV62130?

    We use TLV62130, so we want to know specifications of TLV62130.

    Anyway, regarding resistor divider at EN pin, it ok to use resister value for the divider from kOhms - 10kOhms?

    Moreover, we consider to use Reset IC in order to delay(about:7sec) the detection of En pin.

    What Reset IC do you recommend?

    If there are, please give us the information.

    Regards,

    Tsujita

  • Yes, same EN specifications on TLV62130 and TPS62130. It is fine to use the range you mentioned on the EN resistors. You can use a voltage supervisor like TPS3703 or TPS3890. If you want more details on this, I can also ask the voltage supervisor team to provide options or design assistance. Let me know.

    Thanks,

    Amod

  • Thanks for your kind reply.

    We confirmed the following.

    Case1:After Vin is stable in 5V, we supply EN pin from 0V to 5V (increasing by 0.5V/s).

    We confirmed that Vout outputed when EN pin was about 0.64V. And we confirmed that Vout was good.

    Case2:EN pin is connected with Vin, and Vin supply from 0V to 5V (increasing by 0.5V/s).

    We confirmed that Vout outputed when EN pin was about 2.96V. And we confirmed that Vout dropped like 2ch of the following figure.

    1ch:EN,2ch:Vout

    What the reason is the behavior of Case1 and Case2?

    Regard,

    Tsujita

  • In case 1, EN HI threshold was hit and the IC turned on and regulated. In case 2, since VIN and EN are connected, both EN HI threshold and VIN UVLO threshold needs to be exceeded (around 2.8V or higher) for the IC to turn on and regulate. The scopeshot you attached is quite small but it looks like there is 400mV or so ripple on VIN which carries over to VIN. The rising/falling hysteresis on both these pins for UVLO and EN is around 200mV so it can cause issues. Please confirm how much ripple you have on VIN and see if reducing it makes any difference.

    Thanks,
    Amod

  • Thank you for your reply.

    We understood the behavior about Case1 and Case2.

    We will add Reset IC to control EN pin.

    Regards,

    Tsujita