The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ21701: :

Part Number: LMZ21701
Other Parts Discussed in Thread: TPS62150

Good morning,

I am planning to use LMZ21701 on my design to generate 4 different power rails. 

With TI Webench tool I can't do simulation below 300mA load values. 3 of may voltage rail loads are a round 300mA so they are okay. 

One of my application requires only 30mA continuous from 1V2 voltage rail. My input voltage to LMZ21701 is 5V. 

I see from the datasheet that it is doable. There is also a PWM and PSM modes.

If 30mA falls into PSM mode, then is there going to be a pulse skipping in order to generate the needs? Pulse skipping may have bad impact to EMI?