Other Parts Discussed in Thread: TPS62135
Team,
-Is it possible to use a TPS62147RGXR / TPS62148RGXR on an existing TPS62135RGXR PCB?
All 3 devices have the same VQFN-HR package. The main difference is pin 4 (FB2 on x35 and AGND on x47/x48).
-Is it 100% compatible if FB2 is not being used (ie connected to GND)?
-If FB2 is being used like on Fig 83 SLVSBH3B would the circuit at least work for the default voltage (ie with VSEL LOW)?
-For the LED power supply scenario (Fig 86 of SLVSBH3B and SLVSDR8):
What will happen if FSEL on TPS62147/48 is pulled low like VSEL on TPS62135?
Is it a must to have VSEL HIGH for the LED power use case of fig 86?
Thanks in advance!
A.