This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61240: TPS61240 increasing output voltage...

Part Number: TPS61240

Just for confirmation on the tolerance on the feedback resistors:

Quote: The internal feedback resistor is R1=724k, R2=228K, and the reference voltage is VREF=1.2V. but the variation of the resistor is +-14%

So the absolute tolerance of the resistors is +/- 14%, but the quotient of R2/(R2+R1) is almost constant? R2/(R2+R1) = 228k/(228k+724k) = 0.239

Uout * 0.239 = UREF --> 5V *0.239 V = 1.2V.

Best regards