Dear *,
please can you suggest a device for 50V-200V Boost converter for pulsed discharge application (Adj Out Voltage)
Vin 24V
Vout from 50V to 200V
Iout from 0.3A( for 50V) to 0.075A ( for 200V) [ Pout 15W]
Adjustable output voltage via feedback pin
the output capacitor is 100uF and pulsed load ton max = 100us , toff= T-ton = (1/200Hz) - 100us = 4.9ms
100us discharge time, 4.9ms charge time.
2) if the same inductor and Rs is used for voltages from 50V to 200V, does that mean the the current through inductor for smaller voltages than 200V will be higher before it hits the current limit?
is it somehow possible to adjust the cycle by cycle current limit for smaller output voltages from the outside of the BOOST IC?
Best Regards,
David.