Other Parts Discussed in Thread: BQSTUDIO, , BQ76930, EV2400, BQ76920, BQ78350, BQ78350-R1
Hello,
I am using the EV2400 with the BQ76920EVM and running the bqStudio. My plan was to set any parameters I could now, while waiting for our custom board to be delivered, which will use BQ76930.
However I have now ran into a problem where, following the datasheet I connect 15V, connect through SMBUS and press the Boot button, bqStudio recognises the device for a few seconds but then it goes back to not recognising it. Everything was working normally until I set the cell count to 8. I believe this was the error, as the BQ76920 only supports up to 6 cells. Unfortunately I don't see a way to set it back to 5 cells, as in order to do that I have to reconnect through bqStudio.
If that is not the problem, I don't understand what the problem could be as it was working fine prior to making that change. Any ideas what it could be?
Thank you,
Chris