This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62090: TLV62090 PG pin Absolute maximum ratings

Part Number: TLV62090


Dear All,

About Absolute maximum rating of TLV 62090.
The PG voltage range is 0.3 to Vin + 0.3 V.

However, PG is an open drain output.
Why is the maximum value not an absolute value?