Hi ,
I use the REF5025 for the ADC reference input. In order to reduce the effective noise bandwidth of the reference noise, I added a R which is 6.9kohm in series with the Cout.
Without the 6.9k resistance, the total noise is 46.13uV. With the resistance, diagram shown as below, the total noise got to higher than 300uV.
If I change R1 to be 1.1ohm, the total noise is 67uV. I think based on f_-3dB=1/2*pi*R*C, the higher R goes, the lower the noise bandwidth and the total noise should gets lower. The result is out of my expectation, could you please help with the question?
Besides, if a parallel capacitor 10uF is added, the total noise is reduced to 46.13uV again.
Could you please kindly help with the question?
Thank you so much!
Best regards,
Wendy