Hi,
We are planning to use CSD17484 MOSFET in our design.
it will be used at multiple places,
In one of the circuit, Drain can go up to 15V peak (rarely, typical always stays @ 13.2V), Source is GND, Gate will be driven either 0V or 3.3V.
In this case, sometimes we see VGD is up to -15V (worst case for short time).
I didn't VGSS spec in the datasheet (VGSS - Max VGS with Drain and Source are shorted),
Is the Max Voltage VGD = -15V will problem for this MOSFET (Can i use VGS max specification to compare VGD worst case voltage).