Other Parts Discussed in Thread: BQ24105
Dear team,
Customer are looking for battery charger solution for Coin type lithium battery - ML2020.
Did we have charger solution for this battery? The normal battery voltage is 3V.
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ben,
Is there information for what they will be using to power the charger (what is the Vin)?
Hi Anthony,
The input voltage level is 5V level.
Did we have suitable solution for this application?
Regards,
Hi Ben,
The BQ24105 may be suitable for that voltage as it can be programmed from 2.1V to 15.5V. It's a switchmode charger and has a specified programmable current of 150 to 200 mA.