Hello expert,
May I know recommended operation ambient temperature range for TPS3700? Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ann Lien,
The recommended operating temperature range is -40C to 125C for the TPS3700.
Ben
Hi Ann Lien,
One more thing to add, the TPS3700 consumes very little current and when you calculate the junction temperature of the device at worst conditions (IDD = 13uA, TA = 125C, VDD = 18V, Rtheta-ja = 204.6 C/W) and assuming a 6-pin SOT package, the junction temperature is almost the same as the ambient temperature. See below:
Theta JA = 125C + (VDD*IDD)*(Rtheta-ja)
Theta JA = 125C + (18V*13uA)*(204.6 C/W)
Theta JA = 125.05C
Therefore, the recommended ambient operating temperature can range from -40C to 125C.
I hope this explanation helps answer your question.
Ben
Hello Ben,
Thanks for your detail explanation!
Best regards,
Ann Lien
Hi Ann,
You are most welcome! If you believe I have answered your question, can you please close the thread? Thank you!
Ben