Other Parts Discussed in Thread: LMR33640
Hi Sir,
May I know LM73606 can support 12V convert to negative 5V capability? if yes, please help us to provide reference schematic, thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kuo,
Yes the part can support the conversion from 12V to negative 5V, but the current will be lower than 6A because it is now in the inverting buck boost topology.
We do not have a specific reference schematic but you can follow the guidelines in this app note.
In the app note there is an example using LMR33640 and the idea still the same whether using the LMR33640 or LM73606.
The difference is the current capability for the -5V rail
Alternatively we have a PSPICE model that you can use with PSPICE for TI program
Thanks
-Arief