Other Parts Discussed in Thread: TPS65131
Hi,
I need to design a buck-boost voltage regulator circuit with below specification:
Vin (min)=8V
Vin (max)=38V
Vout= 24V
Iout= 7A
I used TI WEBENCH for the design and simulation. Attaching the link below:
Could you please help me on below queries:
1) can I connect BIAS (Pin-24) to the Output node (Cout) of the regulator circuit ?
2) Number of Input and output capacitors are more, can we reduce the numbers by changing the value to reduce space and cost ? Will it impact the circuit performance ?
3) Any issue or suggestion on the simulated circuit ?