Hi,
We have a system that there's no way to exit ship mode by MR toggling since MR is controlled by MCU which is not powered at this moment. So, we try to exit ship mode through VIN insertion but failed. The detail of the steps is described as below. Please share your inputs regarding how to debug as a next step. Thanks.
What is the voltage level of PMID/CD/MR/IN/BAT before you start to enter ship mode?
- PMID: 3.8V or 5V (depend on with Vin or not)
- CD: could not measure but FW set to high level
- MR: could not measure but FW set to high level
- IN: 0V or 5V (depend on with charge or not)
- BAT: 3.8V
What is test steps to enter ship mode? Simply EN_SHIPMODE bit to ‘1’? Is there anything else you did to enter ship mode?
- Only enter ship mode by Simply EN_SHIPMODE bit to ‘1’
After you enter ship mode, what is the voltage level of PMID/CD/MR/IN/BAT?
- PMID: 3.8V
- CD: could not measure
- MR: could not measure
- IN: 0V (without charge)
- BAT: 3.8V
After you provide a valid voltage to IN trying to exit ship mode but failed, what is the voltage level of PMID/CD/MR/IN/BAT at this moment?
- PMID: 3.8V
- CD: could not measure
- MR: could not measure
- IN: 5V
- BAT: 3.8V
Antony