Other Parts Discussed in Thread: TPS61288
Hello Everyone,
My problem is that I don't know how much power I will receive on the TPS61088 output. Theoretically (according to the datasheet) 30W, but I found on the forum, that you can calculate it and it is much more power than 30 W (https://e2e.ti.com/support/power-management/f/196/p/922733/3410213?tisearch=e2e-sitesearch&keymatch=tps61088#3410213 )
My parameters are as follows:
- Vin = 5 VDC
- Vout = 12 VDC (this supply is for processor COMe)
- Iout = 4-4.5A (this is what I nedd to achieve)
Can you tell me if my condidtions will be met with the TPS61088? Or maybe I need to connect two TPS61088 in parallel (Is it possible? ) ? TPS61088 is in my corporate library, so I try to use it.
Or maybe you can recommend other boost converter that will meet my conditions?
Thank you in advance for your reply! Have a nice day!