Hi,
Im using LM25066 for hotswap application, where i want to put RETRY# into latch off mode.
so i have made RETRY# to pull up with external 3.3V supply, is it ok to connect or we need to connect to VDD only which is coming out from LM25066.
i need same clarification on all strap and control signals.
1. RETRY, CB, CL, Power GOOD, SMBA, Address line and DATA/CLK lines.
Found issue after connecting RETRY# to external 3.3V, FET is showing dead short.
thank you,
Praveenkumar