The datasheet mentions an I_qmax of 600mA when R_REF = 0Ω. Is this an acceptable thing to do? My application needs about 500mA (600 would be acceptable). However, I cannot use a low-side current sense so I cannot use the TL4242 as that seems to be required. However, if I can simply connect REF to GND I will have no current sense to worry about. If this gives me a 600mA output and will not harm the driver, I may be in luck with this part.