This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563210A: Inductor value selection

Part Number: TPS563210A

Hi team,

My customer use 1uH for output inductor on schematic. Our datasheet recommend the value is 1.5uH - 4.7uH.

What is the effect when they use 1uH inductor?

Vin = 8.5 - 17V

Vout = 1.8V

Iout = 2.1A

Best regards,

Hardy Xue