Other Parts Discussed in Thread: TLV704, BQ24610, TPS709
Hi everyone,
I'm using TLV70433 and it's all good and stable.
Here is my working circuit.
The problem is when CE1 disconnected, and Vin have a huge ripple (the photo below).
Even the lowest voltage is still over 15V.
But I got less than 1V on Vout of TLV70433.
Is there any frequency or amplitude of input ripple that make TLV70433 fail?
Thanks